Expansion Modules
Delta OP Control Panel, Recessed
The Recessed version of Delta OP is used where the desired installation in technical desk systems, or where surface-mounted assembly is not appropriate.
The Recessed Version of Delta OP is used where the desired installation in technical desk systems, or where surface-mounted assembly is not appropriate. For recessed mounting builds not the device more than about 5mm outside the surrounding surface. Delta OP satisfies NS-EN-54.2 as a control unit in a fire station network. If the network is to have alarm transmission according to NS-EN54, the OP to be connected to the alarm transmitter must have a kit for alarm transmission for Delta OP.
When upgrading older ANX95 panels, Delta OP can be recessed control panel is installed in the Delta/ANX95 kit for conversion.
Certifications:- NS-EN54