System Configuration Software
FireWin Publisher Server Program
Eltek zone monitor units used to connect conventional detectors that require voltage to operate, S20/S30/S60/S65, etc.
The Eltek zone monitor units used to connect conventional detectors that require voltage to operate, S20/S30/S60/S65, etc. Used as an adapter between conventional signals (on/off) and analogue detector loops. Depending on the signal entering the address unit and the type of address unit will these could give fire, warning or error message to the fire station. They can either be used as an address for a specific signal from, for example, a sprinkler valve, or as a group address when conventional detectors shall be connected to an addressable facility.
Features & Benefits:- Graphic display of building for one safe and fast location of alarm location
- Full overview of the monitored areas
- Possibility of "pop-up" function in Windows