/content/hbtbt/gb/en/search-results.html
li-ion-tamer-hero-banner.jpg
li-ion-tamer-hero-banner.jpg

Best in Class Lithium-ion Battery Protection

Early warning of lithium-ion battery failures and prevention of thermal runaway

Compatible with all lithium-ion battery form factors and chemistries

Li-ion Tamer GEN3 is a plug-and-play rack system that improves safety by sensing the off-gassing that precedes thermal runaway battery failures much earlier than smoke or traditional LFL gas detection would.

Product categories

Li-ion Tamer Gen 3 Gas Sensors

Sensors detect lithium-ion battery electrolyte solvent vapours (off-gas detection), provide temperature and humidity monitoring of the space. Sensors transmit off-gas, temperature, and humidity readings via CANbus to the Hub.

Learn More
Li-ion Tamer Multi Output System UL certified

Assembly comprises Li-ion Tamer G2+ sensor and Interface Module. Provides relays, Modbus 485 and CANbus outputs

Learn More

Recent Updates

Li-ion Tamer Gen2+ Sensor Receives California State Fire Marshal Listing
Learn More
Li-ion Tamer has again made storing energy from lithium-ion batteries safer
Learn More
Off-gas Detection System Receives Favorable Test Result
Learn More
National Lab Testing Demonstrates Value in Early Detection
Learn More

Technology Integration

Discover our high-performance industrial battery pack, designed for durability and efficiency. Featuring a robust metal casing with visible internal cells, this battery pack ensures reliable power for your industrial applications.
Discover our high-performance industrial battery pack, designed for durability and efficiency. Featuring a robust metal casing with visible internal cells, this battery pack ensures reliable power for your industrial applications.

Li-ion Tamer® is designed to provide enhanced safety for your battery systems and can be installed at a wide range of integration points throughout your design. Off-gas begins as gases that are generated inside individual cells due to exothermic reactions which begin to occur as a result of internal problems in the battery or external abuses. The release of these gases is the first stage of a battery failure which can self-propagate until the battery begins to smoke and go into fully developed thermal runaway. The ability to detect the gases provides a signal capable is providing early warning of the eventual cell failure and can enable actions which can help mitigate the effects of the battery failure. Li-ion Tamer® products are designed to detect and protect from individual modules, to EV batteries, to room level integrated solutions.

frequently asked questions

1. What are the stages of Lithium-ion Battery Failure?

Stage 1: Abuse

  • Electrical (over-charge/discharge, or internal manufacturing defects).
  • Thermal (external heating or operating the battery outside its specified temperature).
  • Mechanical (physical damage to the cell).

Stage 2: Initial cell venting (off-gas event)

  • The battery electrolyte will convert to gas increasing the internal pressure and venting to the outside through pressure relief vent or rupture. This gas release is distinctly different than the release of gases at thermal runaway and often occurs several minutes prior to thermal runaway.

Stage 3: Thermal Runaway

  • With increasing internal battery pressure and temperature, the separator will melt down and rupture, releasing smoke and potentially igniting the electrolyte solvent. Thermal runaway enables propagation of abuse and failure to adjacent cells, with any resulting fire further increasing the risk.
2. What gases does Li-ion Tamer detect?
  • Li-ion Tamer is designed to respond to volatile organic compounds (VOCs) which are emitted during a lithium-ion battery off-gas event that occurs prior to thermal runaway. The initial off-gas event consists of primarily battery electrolyte solvent vapours.
  • The off-gas event may also be referred to as the initial cell venting and is defined as the event in which the cell case vents due to a rise in the internal pressure of the cell.
  • Li-ion Tamer will also detect the composition of gases (CO, H2 , hydrocarbons, etc.), released at thermal runaway.
3. Does Li-ion Tamer detect the initial cell venting of different Lithium-ion Chemistries?
  • Lithium-ion battery chemistry refers to anode and cathode chemistry, such as LFP (Lithium Ferro-Phosphate or lithium iron phosphate) or NMC (Nickel Manganese Cobalt).
  • Yes, Li-ion Tamer can detect the initial cell venting (off-gassing) of different lithium-ion battery chemistries. It does this by detecting the presence of battery electrolyte solvent vapours which are common to all battery chemistries. It is agnostic towards the types of anode and cathode chemistries used.
4. How do you stop thermal runaway?
  • Li-ion Tamer can detect off-gassing of different lithium-ion battery chemistries; it does this by detecting the presence of battery electrolyte solvent vapours which are common to all batteries.
  • The off-gas event, or cell venting, is a distinct stage in the stages of a battery failure which occurs prior to the onset of thermal runaway for most forms of battery abuse.
  • Off-gas events are the earliest indicator of thermal runaway and once detected provides sufficient time to initiate containment measures, such as automatically isolating the components of the ESS or otherwise placing it in a safe condition. This action provides a barrier to the onset of thermal runaway.
  • Other mitigating actions can be explored based on system constraints, including increased cooling, local alarms, remote alarms and ventilation activation to remove flammable gas accumulation.
5. How many minutes of early warning does Li-ion Tamer provide?
  • The Li-ion Tamer product typically provides between 2 and 30 minutes warning of a thermal runaway event. The severity of the abuse factor greatly affects the amount of time between the cell venting and thermal runaway.
  • When using the UL 9540A recommended failure method (overheating), Li-ion Tamer consistently delivers early warning with many different types of cell manufacturers, chemistries, and form factors.

Markets We Serve and Beyond

Lithium ion batteries provide power and energy densities demanded by many of today’s energy storage needs. For this reason, lithium ion batteries are being utilized in battery systems across a wide range of markets. Li-ion Tamer® battery monitoring systems are designed with the flexibility of these markets in mind. The operating principles of the monitoring systems are applicable to all lithium ion battery chemistries, form factors, and battery system layouts; they also operate independent of the operational state of the batteries and can even provide valuable monitoring of batteries during shipping and storage.

Crane loading box container to cargo ship at commercial dock port. Shipyard Cargo Container Sea Port Freight forwarding service logistics and transportation. International Shipping Depot
Crane loading box container to cargo ship at commercial dock port. Shipyard Cargo Container Sea Port Freight forwarding service logistics and transportation. International Shipping Depot

Let’s connect

Curious to know more about our solutions? Get in touch or subscribe to our newsletter today.